一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

verlegen (an einen anderen Ort) (v)

displace (v)


The rectangular parallelepiped's edges are displaced at an angle .

This translates into a high load-bearing capacity that resists displacement.

It can withstand no more than 1/3 the displacement force than a Standard Fastener can resist.

move (v)


In such a case, the square nut can be removed from the Multiblock.

If the carriage is to move, a cable chain is required.

If the carriage is to move, a cable chain is required.

relocate (v)


The Counter-Reverse Unit relocates the axis drive from the end of the axis to the carriage.

It relocates the axis drive from the end of the axis to the carriage.

Click 'delete' to remove accessories and 'move' to relocate a centrally mounted Light Fitting to make space for a second Light Fitting, for example.

shift (v)


At the end of the shift, users take their personal items away with them.

However, the hub of computer development shifted to the US.

Further examples of the multiple use of work benches include shift work.

transfer (v)


Die Transfersysteme werden mit den Arbeitsplätzen fest verbunden.

The transfer systems are permanently connected to the work benches.

there is now a logical addition for implementing Transfer Gates.

cambiar (v)

desplazar (v)

mover (v)

reubicar (v)

transferir (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站