一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

壁龛 (n)

Nische (f)


Vor Erreichen der mechanischen Endlage wird automatisch gestoppt.

Gleiches möchten wir nun auch mit einer spanischen Version starten.

Mechanische Werte (gelten nur in Pressrichtung)Zugfestigkeit Rmmin.

extension (n)


Simple clamping technology for rapid reconfiguration, disassembly and extension.

Heijunka means smoothing and therefore describes an extension of levelling in production.

Additional extensions can be added anywhere with the flick of a wrist.

niche (n)


However, there are other niche areas where a varied range of work bench types are used.

Niche applications for work benches can also include dental technology, goldsmithing and watchmaking.

recess (n)


The Captive Nuts can be installed by snapping the latch springs into the corresponding recess.

As a result, they run on the top and underside of the recess in the support profile.

The closed rear wall of the Recessed Grip prevents the operator's fingers from extending all the way through and possibly being injured.

extensión (n)

nicho (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站