一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

中间的 (n)

Mitte (f)


Die Schalter werden mittels Klemmung in der Aufnahmenut gehalten.

Am Arbeitsplatz wird mittelgrobe oder Präzisionsarbeit gefordert.

Montiert werden diese mittels Innsensechskant-Schlüssel der SW 5.

center (n)


Die ausgewählten Artikel können Sie direkt im Downloadcenter zum Download ablegen.

and to put the chosen parts directly in the download center for downloading.

The awards ceremony took place on the opening day of CeBIT at the Hannover Exhibition Center.

centre (n)


In the case of a body-fixed system of coordinates, a polhode is used to depict instantaneous centres of rotation.

When the frame of reference is fixed on the body, a moving centrode (also known as a body centrode) depicts the instantaneous centres of rotation.

A centre mark on the Fastener makes it easier to build frames.

middle (n)


Roller bearings with rollers in the upper part and a steel tenon (the centre pin) in the middle.

They comprise a middle part known as the web and a horizontal part (flange) at both the top and bottom.

The middle part of the workpiece can be shaped more extensively and better cold hardening achieved.

centro (n)

medio (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站