一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

Magnetanker (m)

armature (n)


When the excitation field and load torque are constant, the armature current decreases when the armature voltage is reduced.

The stator in these machines is equipped with an AC winding that generates an alternating magnetic field using an armature that usually has a squirrel cage design.

In theory, the stator windings can be replaced with two counter-rotating DC windings, while the function of the armature corresponds to two counter-rotating rotors.

armadura (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站