一种定义
四种语言
In Festlagern (3-wertig) ist der Stab immer tangential anliegend.
Das Festlager muss auf der Antriebsseite der Transportrolle liegen.
Gleitführungen mit mehreren Gleitschlitten müssen als Kombination aus Festlager (F) und Loslager (L) ausgeführt werden.
The fixed bearing must be positioned on the drive side of the Conveyor Roller.
Slide guides with several slides must be designed as a combination of fixed bearing (F) and floating bearing (L).
Fixed bearings facilitate moments in all three directions and also absorb transverse forces and normal force.
In fixed supports (valency of 3), the member is always tangentially adjacent.
Fixed supports permit moments in all three dimensions and carry both transverse forces and normal force. They have a valency of 2.