一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

hindern (v)

hamper (v)


Long cables and hoses that hamper work are a thing of the past.

Long cables and hoses that hamper work are a thing of the past.

impede (v)


This impedes uniform charge carrier motion - the current flow.

The results are health and safety solutions that don't impede working processes, are quick to assemble and can be repeatedly reconfigured.

Sound insulation is designed to impede or prevent the propagation of airborne and solid-borne sound by reflecting it as it crosses between two media.

inhibit (v)


Because this approach shifts the focus onto short-term gains, it inhibits the development of a culture that promotes continuous improvement.

This inhibits a culture of continuous improvement, where every employee consciously contributes to a corporate culture that is permanently seeking to improve everything.

In the cold range, a person's sense of wellbeing can be affected even if conditions are only slightly outside the comfortable range, because low temperatures inhibit the blood flow to the skin and extremities.

obstruct (v)


Obstructing dislocation movements has a negative impact on toughness.

The profile grooves facing each other inside the frame remain unobstructed so they can be used for holding panel elements.

impedir (v)

obstaculizar (v)

obstruir (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站