一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

fertig (adj)


Die Trittplatte ist aus einem ableitfähigen Kunststoff gefertigt.

Der Schlitten wird auf das fertig konfektionierte Profil geschoben.

Klick und fertig - so einfach kann das Montieren einer Strebe sein.

complete (adj)


This risk can be mitigated, but not completely eliminated.

I will complete my details at a later point in time.

When everything is in easy reach, work can be completed much faster.

completed (adj)


When everything is in easy reach, work can be completed much faster.

A fully assembled Linear Unit KRF is a partly completed machine.

However, such elements may only be incorporated once all backlash adjustments have been completed.

done (adj)


This can be done using side lighting, for example.

What's more, work that previously had to be done by two members of staff can often be done by just one.

Simply drill through the plate and secure it with T-Slot Nuts - job done.

finished (adj)


How are the finished products transported away from the work bench?

They are used either as end products or as semi-finished products for further processing (e.g. lamination).

Goods, finished parts and consumables - in a modern production system everything has to keep flowing.

off-the-shelf ... (adj)

ready (adj)


Indeed, some regions are already experiencing a shortfall in workers.

We've already calculated the pretensioning that we need in the belt.

The roller tool is now ready to start beading the upper ribs.

ready-made ... (adj)

... de mostrador (adj)

acabado (adj)

completado (adj)

completo (adj)

hecho (adj)

listo (adj)

进一步查找


item


访问 item 官网
我们的新网站

去網站