一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

易延展的 (adj)

dehnbar (adj)

ductile (adj)


The ductile yield is a value that indicates a material's ductility.

Rigid materials such as steel have a higher modulus of elasticity than ductile materials.

It can be used for materials or components with ductile properties.

elastic (adj)


Tensile testing provides one example of elastic behaviour.

A material's rigidity can be indicated by the modulus of elasticity.

Tensile tests are used to determine the modulus of elasticity E in experiments.

extensible (adj)

flexible (adj)


The ends of the Warning and Protective Profiles are sealed by flexible Caps.

The flexible impact protection covers over profile edges and sides.

Flexible Conduit E is added as a work bench feature.

dúctil (adj)

extendible (adj)

flexible (adj)

进一步查找


item


访问 item 官网
我们的新网站

去網站