一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

绳 (n)

Seil (n)


Grummets sind endlos gemachte Seile, sie zählen zu den Anschlagseilen.

Damit ein schlaffes Seil nicht abspringt, werden Schutzkästen montiert.

Keine Kollision oder Reibstellen zwischen Zugseil und Pneumatikschlauch.

cable (n)


If the carriage is to move, a cable chain is required.

Conduit Inside Corners, Conduit Caps and Cable Entry Protectors - Safe cornering.

It can also be used to safely cover over cables that have been routed through a groove.

cord (n)


A person's physical strength will also vary according to their age, body size, weight and gender.

The components were arranged according to a specific modular dimension.

The subsequent installation sequence varies according to the circumstances.

rope (n)


The tread plate is made from a plastic with ESD (electrostatic discharge) properties.

Material properties are a material's parameters.

They can also be used to change material properties.

cordón (n)

cuerda (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站