一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

合规 (n)

Einfederung (z.B. Feder) (f)

compliance (n)


The door can be opened and closed in full compliance with machine design directives.

Systematic quality management ensures complete compliance with agreed standard values.

The strength of rolling friction varies according to the surface attributes, compliance and hardness of the rolling element and surface.

contraction (n)


This elongations a right angles to the direction of traction is called lateral contraction.

This narrowing is referred to as lateral contraction, which is dependent on the Poisson ratiov.

The Poisson number is a dimensionless parameter for a body's lateral contraction under a tensile stress.

deflection (n)


However, deflection in the Shaft is even more important.

Profile deflection caused by the inherent load and the load from the assemblies.

Profile deflection in very wide work benches due to the weight of the bench itself.

resilience (n)

spring compression (n)

compresión de resorte (n)

contracción (n)

cumplimiento (n)

deflexión (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站