一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

检查 (n)

Kontrolle (f)


Hier wird Ihnen zur Kontrolle eine Vorschau Ihres Systemmobils angezeigt.

Sichtkontrolle, ob alle Zahnstangensegmente einander stirnseitig berühren.

Kleine, genaue Bewegungen, die viel Augenkontrolle verlangen, werden am besten in Zone 1 angeordnet.

check (n)


Also check the maximum load-carrying capacity of the Threaded Inserts.

The same logic is then applied as with check count 1.

The stocktaking manager then also checks whether all stocktaking locations have been covered.

check-up (n)


An acclimatisation phase after occupational medical check-ups can help to reduce the stress associated with working in hot ranges.

examination (n)


Because value analysis - as a retrospective examination - uses the same tools as design engineering, the two processes complement each other.

monitoring (n)


Die Methodik erfordert nicht nur eine rigorose Überwachung aller Arbeitsschritte mit permanentem Monitoring und Feedback.

As a methodology, it demands that companies keep a close eye on all work stages, ensuring continuous monitoring and feedback.

The following basic principles for a proper inventory need to be complied with when planning, performing, monitoring and evaluating the inventory.

verification (n)

examinación (n)

monitoreo (n)

revisión (n)

verificación (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站