一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

曲线 (n)

Kennlinie (f)


Im Arbeitsbereich der Z-Dioden verlaufen die Kennlinien nahezu linear.

Die Rückwärts-Sperrkennlinie entspricht im Wesentlichen der einer Diode.

Die Regelkennlinie wird auch statische Kennlinie der Regelstrecke genannt.

characteristic (n)


The characteristic curves are almost linear in the Zener diodes' operating range.

The reverse off-state characteristic is essentially the same as that of a diode.

It is also called the static characteristic of the controlled system.

characteristic curve (n)


The characteristic curves are almost linear in the Zener diodes' operating range.

In the positive control direction, there are two characteristic curves - the blocking characteristic and the on-state characteristic.

Consequently, each input variable x corresponds to a fixed output variable y. The output variable y can be depicted via the input variable x in the component's characteristic curve.

curve (n)


The characteristic curves are almost linear in the Zener diodes' operating range.

The curve can be used to determine the stability of closed-loop control systems.

The component does not fail in the area below the curve.

característica (n)

curva (n)

curva característica (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站