一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

旋转中心 (n)

Drehpunkt (m)


Das Moment an jedem Ausleger, in Abhängigkeit dessen Abstand vom Drehpunkt muss errechnet werden.

center of rotation (n)

centre of rotation (n)


The point where the relevant perpendiculars of two velocity vectors intersect is the instantaneous centre of rotation.

At this specific instant, the movement can be replaced by an infinitesimally small moment around the instantaneous centre of rotation.

The centre of rotation is located at the top of the Angle Bracket.

fulcrum (n)

pivot (n)


This ensures that the pivot frame can be used on both sides.

Pivot Arms can only be fitted to vertical profiles that incorporate a groove.

Left-click the mouse at this position to insert the Pivot Arm.

centro de rotación (n)

fulcro (n)

pivote (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站