一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

上限 (n)

Obergrenze (f)

ceiling (n)


The ceiling construction reaches from one side of the room to above the operating table.

The ceiling mount can be seen in the background, running from left to right into the room.

The ceiling mount made of MB profiles was installed in next to no time and the mobile camera was almost ready for use.

maximum level (n)

upper limit (n)


In this case, the actual value oscillates around the setpoint value, because the manipulated variable jumps to '1' if it falls below a certain value and to '0' if it exceeds the upper limit value.

límite superior (n)

nivel máximo (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站