一种定义
四种语言
If the carriage is to move, a cable chain is required.
Conduit Inside Corners, Conduit Caps and Cable Entry Protectors - Safe cornering.
It can also be used to safely cover over cables that have been routed through a groove.
Everything from the most awkward corner to large cabins can be lit up.
The under-bench cabinet is ideal for storing tools or housing a PC or other components.
The model is subsequently hardened in a hardening cabinet until it reaches its final strength.
If the carriage is to move, a cable chain is required.
Slide the prepared carriage onto the support rail.
The closed side panel gives the Angle Bracket its high load-carrying capacity.
The lift carriage in the inner frame also runs on rollers.
Guide rollers are mounted on the two vertical sides of the lift carriage.