一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

客运车厢 (n)

Wagen (m)


Demgegenüber werden handbetriebene Hochhubwagen selten eingesetzt.

Sie können auf einer Laufbahn am Unter- und am Oberwagen abrollen.

Der Handgabelhubwagen gehört zu den handbetriebenen Flurförderzeugen.

car (n)


If the carriage is to move, a cable chain is required.

Slide the prepared carriage onto the support rail.

The closed side panel gives the Angle Bracket its high load-carrying capacity.

carriage (n)


If the carriage is to move, a cable chain is required.

Slide the prepared carriage onto the support rail.

If the carriage is to move, a cable chain is required.

coach (n)


Der Erste ist der Master Black Belt (Trägers des schwarzen Gürtels), der als Coach, Trainer und Ausbilder wirkt.

At the top of the hierarchy is the Master Black Belt, who acts as the head coach.

truck (n)


Manually operated high-lift pallet trucks are rarely used.

Counterbalance fork-lift trucks are motorised floor conveyors.

They are used to transport pallets and to load/unload trucks.

vehicle (n)


Positional coordinates are measured constantly to control the vehicle movements.

All eight wheels are steered via hydraulic cylinders on the vehicle sides.

In automated guided vehicle (AGV) systems, floor conveyors operate automatically.

camión (n)

carro (n)

coche (n)

vehículo (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站