一种定义
四种语言
Die Transfersysteme werden mit den Arbeitsplätzen fest verbunden.
Unterschieden werden gleisgebundene und gleislose Flurförderzeuge.
Verbundmaterial ist schubsteif und hat hohe Biege- und Knickfestigkeit.
Application 3: supplied square nut is inserted into both collar halves.
The upper surface of the slide has been milled flat and features four openings for positioning collars.
When the clamp collars are aligned in parallel, this indicates that the screw connections are correctly pre-tensioned.
The Flange can also be screwed directly to the Support Arm, however.
Depending on the application, the drive cannot always be directly flange-mounted.
Wheel flanges or horizontal guide rollers keep the travelling wheel on the rails.
This roughly equates to shoulder height, depending on the size of the user.
Moreover, the chair should allow sufficient room for movement in the shoulder area.
Arm rests relieve strain on the shoulder and upper arm muscles and also improve steadiness in the hands.