一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

Überprüfung (f)


Die automatische Überprüfung Ihrer USt.-IdNr. war leider nicht möglich.

Zur Überprüfung der ESD-gerechten Ausführung genügt es, den Ableitwiderstand zu messen.

Probefahrt mit Überprüfung der Endanschläge und der Funktion eventueller Sicherheits-Endschalter /-Verriegelungen.

audit (n)


Schall sind Geräusche, Töne und Klänge, die auditiv mit dem Ohr-Gehirn-System wahrgenommen werden.

Sounds are noises that can be picked up by the auditory system.

check (n)


Also check the maximum load-carrying capacity of the Threaded Inserts.

The same logic is then applied as with check count 1.

The stocktaking manager then also checks whether all stocktaking locations have been covered.

examination (n)


Because value analysis - as a retrospective examination - uses the same tools as design engineering, the two processes complement each other.

inspection (n)


This lab work bench was developed for the inspection of windscreens.

Carry out a visual inspection to ensure that the end surfaces of all of the Rack Segments meet.

The planned period of use and frequency of inspections are also to be given due consideration.

review (n)


A preview of your SystemMobile is displayed for you to check.

Please don't write your questions in reviews, as we are unable to respond to them in this format.

The currently selected dimensions are shown in bold in the preview.

verification (n)

auditoria (n)

examinación (n)

verificación (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站