一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

紧挨着 (adj)

neben (adj)


Kleine Abmaße zur direkten Montage neben einer senkrechten Strebe.

Es wird in die Nut nebeneinanderliegender Stufenprofile eingeschoben.

Daneben ist sogar noch ausreichend Platz für handschriftliche Notizen.

adjacent (adj)


In fixed supports (valency of 3), the member is always tangentially adjacent.

Small dimensions enable installation directly adjacent to a vertical strut.

It is inserted into the grooves of adjacent Step Profiles.

alongside (adj)


However, SystemMobiles L don't just shape up well when used alongside work bench systems.

Freely positionable products are shown alongside the mouse pointer immediately after being selected.

Tools that are used rarely can be placed around the periphery or alongside auxiliary elements.

close to (adj)


If a company is to get close to achieving this goal, the most important thing it can do is massively reduce setup times.

The plate has been designed in these dimensions so that the struts can be installed as close to the wall as possible.

The measured values lie close together but their mean value may deviate from the true value.

near (adj)


The linear guide system is best placed to accommodate this type of torque.

Linearsysteme müssen perfekt auf die Aufgabe zugeschnitten werden.

Linear systems need to be perfectly configured for the task at hand.

neighbouring (adj)


Neighbouring work benches often need to be interlinked by an easy-to-use system.

Earthing Connection 8 can also be used to interconnect neighbouring shelves or table constructions in order to equalise potential.

Vibrations in the ground caused by neighbouring machinery and plants must not result in short or long-term disruption to series production.

next to (adj)


Quick-action couplings at the ends of the hose ensure the system can be connected up in next to no time.

Using T-Slot Nuts allows heavy-duty fastenings to be created in next to no time.

The angle of the trays can be adjusted in next to no time without the need for tools.

adyacente (adj)

al lado de (adj)

cerca (adj)

junto a (adj)

vecino (adj)

进一步查找


item


访问 item 官网
我们的新网站

去網站