一种定义
四种语言
Fahrwerke werden zur Fortbewegung von Fördermaschinen eingesetzt.
Extreme Belastungen des Bewegungsapparates werden somit reduziert.
Unnötige monotone Bewegungen müssen durch Planung vermieden werden.
During this infinitesimally short moment in time, it is motionless.
The tilting motion determines the path of motion of the goods as they are ejected.
In this state, the body is either motionless or moves at a uniform speed in a straight line.
Planning must ensure that unnecessary, monotonous movements are avoided.
Movement along the X axis is controlled by two synchronised KLE 8.
Positional coordinates are measured constantly to control the vehicle movements.
They can travel at speeds of up to six kilometres per hour.
Due to high wheel forces, travelling wheels installed in cranes have broad running surfaces.
The travelling wheels of very large cranes are often driven individually.