一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

轴 (n)

Radachse (f)

axis (n)


As a result, the entire guide axis is compact and sealed.

When using an axis with a stroke of 1 metre, that's the equivalent of 5 million double strokes.

Movement along the X axis is controlled by two synchronised KLE 8.

axle (n)


easy-running roller conveyors with steel axles for a long service life.

The hook crossmember is connected to the cable pulley axle by supports.

The point at which axle travel/belt elongation begins must first be found.

gear axis (n)

wheel axis (n)

eje (n)

eje de engrane (n)

eje de rueda (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站