一种定义
四种语言
Acceleration a is calculated based on the path/time rule.
The tilting motion determines the path of motion of the goods as they are ejected.
Path s applied over time t is described by a parabola.
Plastic wheel rim that leaves no visible tracks behind it.
They can roll against a track in the lower part and upper part.
In case of unforeseen events, a tailhook secures the track guidance.
A force that is applied perpendicular to the trajectory does not result in any work on the body.
In mathematical terms, the unit tangent vector is the derivation of the trajectory over time.
In the following section of the trajectory, this is converted back into kinetic energy.