一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

紧固的 (n)

Befestigung (f)

attachment (n)


Slimline Line 6 Profiles for fastening lightweight attachments.

Attachments can be screw connected in all three spatial directions.

The trucks can be equipped with various load-handling attachments.

fastening (n)


Fastening Disc M5 is provided with a threaded blind hole.

So it should not be used for profile connections in combination with fastening elements.

So it should not be used for profile connections in combination with fastening elements.

fixing (n)


Hinges St for fixing solid panels to profile frames.

Their only purpose is to act as an axial fixing for the Rack Segments.

It's the Fixing Clip that will hold it together after installation.

mounting (n)


Place the pulley over the guide pin onto the mounting plate

The Slide Profiles allow users to locate mounting bores at will.

The working height of the mounting plate is ideal for standing work.

acoplamiento (n)

montaje (n)

sujeción (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站