一种定义
四种语言
The workpiece is disassembled and the parts placed in containers.
Several struts have to be fastened in place or unfastened at the same time - meaning the entire structure has to be rebuilt or disassembled.
This means that the individual components of the various units can be disassembled later for recycling.
This provides an effective means of preventing a closed door from being dismantled.
Everything that has to be dismantled can be reused in some other way.
The Clamp Strips and the panel elements can be retrofitted into the profile frame and also be dismantled again.
In such a case, the square nut can be removed from the Multiblock.
Transported materials can be easily removed from shelves.
Remove Carriage Profile KLE section from the press-fit device