一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

特征 (n)

Kurve (Kennlinie) (f)

bend (n)


Der Online-Shop richtet sich an Unternehmen und Gewerbetreibende.

This process involves tensile and bending deformation.

Fräsen ist ein spanabhebendes Trennverfahren für feste Werkstoffe.

characteristic (n)


The characteristic curves are almost linear in the Zener diodes' operating range.

The reverse off-state characteristic is essentially the same as that of a diode.

It is also called the static characteristic of the controlled system.

curve (n)


The characteristic curves are almost linear in the Zener diodes' operating range.

The curve can be used to determine the stability of closed-loop control systems.

The component does not fail in the area below the curve.

característica (n)

curva (n)

doblez (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站