一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

滑动摩擦 (n)

Gleitreibung (f)

dynamic friction (n)

kinetic friction (n)


A body can be subjected to kinetic friction on both a level surface and an inclined surface.

The kinetic friction force FK travels in the opposite direction to the sliding body and parallel to the sliding surface.

A body on an inclined plane will move down the slope if the downhill force FD is greater than the kinetic friction force FK.

sliding friction (n)


They can be fitted into the profile grooves, are hard-wearing and have a low coefficient of sliding friction.

The Slide Strips serve as slide elements when transporting goods or workpiece carriers, for example. They can be fitted into the profile grooves, are hard-wearing and have a low coefficient of sliding friction.

fricción cinética (n)

fricción por deslizamiento (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站