一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

旋转 (n)

Drehen (n)


Der Gewindeschneidkopf führt die drehende und die lineare Bewegung aus.

Einstellschraube mit linksdrehendem Feingewinde zum Einstellen der Loslagerseite.

Den Stundenzeiger weiterdrehen, bis eine Zeit zwischen 3 und 9 Uhr eingestellt ist.

rotate (v)


The honing tool either moves along the longitudinal axis or rotates.

Depending on the particular application, it may be necessary to rotate the spacer washers in the housing.

Ideally, the seat should dip forward slightly and rotate.

turn (v)


The return height of the tool can be adjusted as required.

The return stroke (non-cutting stroke) returns the tool to the starting position.

Additional stopper can be used to adjust the return height

turning (n)


Consequently, the floating bearing is secured by turning to the right, as usual.

Adjusting screw with left-turning fine thread for adjusting the floating bearing side.

Improvement, increased efficiency and innovation are what keep the wheels of the economy turning.

girando (n)

girar (v)

rotar (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站