一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

弧 (n)

Bogen (m)


In Lichtbogen-Öfen wird Stahl zur weiteren Verwendung eingeschmolzen.

Beim Schruppen werden meist gerade oder gebogene, zum Schlichten spitze Meißel verwendet.

Der Anfragebogen im Internet wird überarbeitet und wird dann für beide Baureihen nutzbar sein.

arc (n)


Electric arc furnaces are used to melt steel for further processing.

Herzogsägmühle is a very special place, where inclusion is part and parcel of everyday life.

FIBEPA supplies optical analytical equipment for the research sector and industry.

arch (n)


FIBEPA supplies optical analytical equipment for the research sector and industry.

They can be tailored to the needs of customers in industry and research in a variety of ways.

It can be built to any length and has no overarching structures or elements above it.

bow (n)


Steel continuous casting systems are available as vertical, vertical turn-out, circular-arc and oval-bow machines.

In addition to vertical and vertical turn-out machines, there are also circular-arc and oval-bow systems, which enable a far lower construction height.

curvature (n)


The circle of curvature has a centre of curvature M and a radius r, which is referred to as the radius of curvature.

The size of the circle of curvature is also important when determining distortion caused by the effect of a bending moment.

First, take a look at the steel strip. You'll notice that it has a slight curvature, which is a result of the manufacturing process.

curve (n)


The characteristic curves are almost linear in the Zener diodes' operating range.

The curve can be used to determine the stability of closed-loop control systems.

The component does not fail in the area below the curve.

arco (n)

curvatura (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站