一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

喷雾 (v)

spritzen (v)

injection-mould (v)

paint (v)


Check that the substances you are using are suitable for use on paints and plastics.

If necessary they can be painted a specific colour.

Any customer can have a car painted any color that he wants so long as it is black.

spray (v)


The guide system must be re-lubricated using the spray can.

We have the solution - in the form of the Cup Holder, which is also ideal for storing spray lubricants, cleaning agents and so on.

The process of inserting the Coupling Insert into the Coupling Halves can be facilitated by using spray oil.

moldear por inyección (v)

rociar (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站