一种定义
四种语言
Ist der Arbeitsplatz in das Datennetz integriert, ist auch eine elektronische Kennzeichnung erforderlich, die mit der räumlichen Kennzeichnung übereinstimmen muss.
Agreed deviations are to be documented as changes to the contract.
All agreements with the Contractor are to be confirmed in writing to the Customer.
Any potential change in the claim for remuneration is to be checked and, if necessary, agreed separately.
It is important to ensure that the holes in the Cover Plate coincide with ??? the threads in the Slide and that the gap is symmetrical.
It is important to ensure that the holes in the Cover Plate coincide with the threads in the Slide and that the gap is symmetrical.