一种定义
四种语言
Das Ziel der sogenannten Wertstromanalyse (value-stream mapping, VSM) ist, die Durchlaufzeiten zu optimieren und einzelne Arbeitsschritte genau zu takten.
Continue to turn the crown until the hour hand lies somewhere between 3 and 9 o'clock.
The tensioning mechanics are designed so that turning clockwise tightens the belt.
Turn the two eccentric bolts anticlockwise slightly and tighten the lock nuts by hand.
Quick-action couplings at the ends of the hose ensure the system can be connected up in next to no time.
This innovative approach cuts assembly time and saves a great deal of space in machinery.
An electrically conductive connection is established at the same time.