一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

变压器 (n)

Wandler (m)


Diese wird über den Schallwandler (Konverter) in mechanische Schwingungsenergie (Ultraschall) umgewandelt.

Das sind elektrothermische Wandler, die aus dem Kontakt zweier unterschiedlich dotierter Halbleiter bestehen.

Typische Anwendungen für OV sind Impedanzwandler, Summierverstärker, Pegelumsetzer, Integrierer und Differenzierer.

converter (n)


This electrical energy is converted into mechanical vibrational energy (ultrasound) by the sound converter.

These are thermoelectric converters that harness the contact between two differently doped semi-conductors.

Key applications include switched-mode power supplies, frequency converters, direct DC converters and inverters.

transducer (n)


Tachogenerators and eddy current transducers use this principle.

Inductive displacement transducers are manufactured and used based on this property.

Resistive displacement transducers or measured value potentiometers use ohmic resistance and a moving arm.

transformer (n)


An isolating transformer separates the operating circuit from the supply system.

Single-phase transformers are used very frequently in electrical household appliances.

Electronic Transformers should be selected as appropriate to the output of the relevant light fitting.

convertidor (n)

transductor (n)

transformador (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站